Part Number: TM4C1290NCPDT
- Is it possible to use the M0PWM0,1 and 7 (Pin 6,43,44) to output a 16bit pwm with same frequency but different duty cycle?
- Is it possible to measure the time of a period of a input frequency at Pin 86 (T0CCP1)?
- ROM Bootloader can be invoked at UART (Pin33/34)?
- Can the microcontroller used without a 25 MHz crystal and will be still usable for 230400 Baud UART?