Hi,
I'm porting a C++ application from a Linux platform, to run under TI RTOS. If possible, I would like to use a std::mutex.
Adding:-
#include <mutex>
compiles OK, but as soon as I try and declare a
std::mutex myMutex;
it just says namespace std does not include mutex.
I have tracked down the header file in
C:\ti\ccs1040\ccs\tools\compiler\ti-cgt-arm_20.2.5.LTS\include\libcxx
and see that the first section, including namespace std, is commented out, but the later bits include _mutes_base and this seems to define std via the macro _LIBCPP_BEGIN_NAMESPACE_STD.
Ideally, to minimise change, I would like to use
std::lock_guard<std::mutex> lk(myMutex);
but getting just the mutex working would be a good start.
Any tips?
Thanks
Jim