Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2432: General Queries

Part Number: AM2432

Hi, I am planning to use AM2432 micro controller for my project. I have some queries about the controller interface

  • Can all the 5 SPI controllers use independently at the same time?
  • What is the maximum speed possible by CAN bus (not FD)?
  • Does each single core cluster of Arm cortex-R5F can work with 800MHz
  • Is there any turbo frequency available?
  • How much can be the power consumption of each cores? can we shut off single core?
  • How many Parallel interface can be connect to GPMC?
  • How the communication between the two cores
  • What is the application for Real time Programmable unit
  • How many Gb Ethernet ports are available. I saw 2 Ethernet ports (under General connectivity) and 2xGMAC under industrial connectivity
  • How this micro controller is different from AM64x series