Part Number: TM4C1294KCPDT
Hi forum,
Why TT3 (105°C) loads 3v3 LDO 2.92v yet DTi3 (85°c) LDO maintains 3v329 installed in the same PCB layout component structures does not. Also notice DTT3 EMI is less guarded where DTi3 seems immune to same EMI source. What makes DTi3 be immune to same EMI source in the same PCB layout structures as DTT3 resides? Note the 3v3 LDO was also replaced on DTT3 PCB but has same load 2v92 occurs.
When the DTT3 has same EMI peak source as DTi3 it dead locks CPU refusing to reset by push button, must POR the MCU. Yet when the DTT3 EMI magnitude is reduced below DTi3 peak EMI it runs application and peripherals as expected. Why does the DTT3 refuse to reset by user push button when CPU locks up?
The running watch dog does not reset DTT3 when EMI reaches a peak magnitude it (ADC/CPU) just locks up. Whereas the DTi3 watchdog would indeed reset the CPU upon same peak magnitude EMI source that locks the DTT3.
Happy Holidays