Part Number: EK-TM4C123GXL
Other Parts Discussed in Thread: TM4C123GH6PM
I want to do ADC calculation on EK-TM4C132GXL development board. But I want to do this calculation using PWM signal. In short, every time the PWM signal is at the rising edge, I want the ADC to trigger and take a sample at that time and continue this process, but I could not do this, can you help me?
#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "driverlib/debug.h"
#include "driverlib/sysctl.h"
#include "driverlib/adc.h"
#define TARGET_IS_BLIZZARD_RB1
#include "driverlib/rom.h"
#include "driverlib/sysctl.h"
#include "driverlib/pin_map.h"
#include "driverlib/gpio.h"
#include "driverlib/pwm.h"
uint32_t ui32ADCAvg=0;
uint32_t ui32ADC0Value[8] = {0};
uint32_t ui32Load=0;
int cnt=0;
void handler_ADC(void);
void ADC_init(void);
void PWM_init(void);
int main(void)
{
// Set the System clock to 80MHz and enable the clock for peripherals ADC0 and GPIO PortB
SysCtlClockSet(SYSCTL_SYSDIV_2_5|SYSCTL_USE_PLL|SYSCTL_OSC_MAIN|SYSCTL_XTAL_16MHZ);
//handler_ADC();
PWM_init();
ADC_init();
while(1)
{
// Clear the ADC Interrupt (if any generated) for Sequencer 0
//ADCSequenceDataGet(ADC0_BASE, 1, &ui32ADC0Value[0]);
/*ADCSequenceDataGet(ADC0_BASE, 1, &ui32ADC0Value[1]);
ADCSequenceDataGet(ADC0_BASE, 1, &ui32ADC0Value[2]);
ADCSequenceDataGet(ADC0_BASE, 1, &ui32ADC0Value[3]);
ADCSequenceDataGet(ADC0_BASE, 1, &ui32ADC0Value[4]);
ADCSequenceDataGet(ADC0_BASE, 1, &ui32ADC0Value[5]);
ADCSequenceDataGet(ADC0_BASE, 1, &ui32ADC0Value[6]);
ADCSequenceDataGet(ADC0_BASE, 1, &ui32ADC0Value[7]);*/
// Trigger the ADC Sampling for Sequencer 0
//ADCProcessorTrigger(ADC0_BASE, 1);
// Wait the program till the conversion isn't complete
// while(ADCIntStatus(ADC0_BASE, 1, false));
// Store the values in sequencer 0 of ADC0 to an Array
// Calculate the Average of the Readings
}
}
void ADC_init(void)
{
SysCtlPeripheralEnable(SYSCTL_PERIPH_ADC0);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOE);
//SysCtlADCSpeedSet(SYSCTL_ADCSPEED_250KSPS);
// Enable hardware averaging on ADC0
ADCHardwareOversampleConfigure(ADC0_BASE, 64);//
// Configure to use ADC0, sample sequencer 0, processor to trigger sequence and use highest priority
ADCSequenceConfigure(ADC0_BASE, 0, ADC_TRIGGER_PWM0, 1);
// Configure PB4 as Analog Input Pin
//GPIOPinTypeADC(GPIO_PORTE_BASE, GPIO_PIN_3);
// Configure all 8 steps on sequencer 0 to sample temperature sensor
ADCSequenceStepConfigure(ADC0_BASE, 1, 0, ADC_CTL_CH0 );
ADCSequenceStepConfigure(ADC0_BASE, 1, 1, ADC_CTL_CH0 );
ADCSequenceStepConfigure(ADC0_BASE, 1, 2, ADC_CTL_CH0 );
//ADCSequenceStepConfigure(ADC0_BASE, 1, 3, ADC_CTL_CH0 );
/*ADCSequenceStepConfigure(ADC0_BASE, 1, 4, ADC_CTL_CH0 );
ADCSequenceStepConfigure(ADC0_BASE, 1, 5, ADC_CTL_CH0 );
ADCSequenceStepConfigure(ADC0_BASE, 1, 6, ADC_CTL_CH0 );*/
// Mark as last conversion on sequencer 0 and enable interrupt flag generation on sampling completion
ADCSequenceStepConfigure(ADC0_BASE, 1, 3, ADC_CTL_CH0|ADC_CTL_IE|ADC_CTL_END);
ADCIntEnable(ADC0_BASE, 1);
ADCIntRegister(ADC0_BASE, 1, handler_ADC);
// Enable Sequencer 0
ADCSequenceEnable(ADC0_BASE, 1);
//ADCIntClear(ADC0_BASE, 0);
//ADCIntEnable(ADC0_BASE, 0);
//IntEnable(ADC_INT_SS0);
ADCProcessorTrigger(ADC0_BASE, 1);
}
void PWM_init(void)
{
// Initialise PB7 M0PWM1
SysCtlPWMClockSet(SYSCTL_PWMDIV_1); // clock defined in sysctl.c
SysCtlPeripheralEnable(SYSCTL_PERIPH_PWM0); // TM4C123GH6PM has two modules (0 and 1)
//SysCtlPeripheralEnable(SYSCTL_PERIPH_PWM1); // TM4C123GH6PM has two modules (0 and 1)
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
//GPIOPinTypePWM(GPIO_PORTB_BASE, GPIO_PIN_7);
GPIOPinTypePWM(GPIO_PORTB_BASE, GPIO_PIN_6);
GPIOPinConfigure(GPIO_PB6_M0PWM0);
//GPIOPinConfigure(GPIO_PB7_M0PWM1);
//IntEnable(INT_PWM0_0_TM4C123);
PWMGenConfigure(PWM0_BASE, PWM_GEN_0, PWM_GEN_MODE_UP_DOWN | PWM_GEN_MODE_NO_SYNC);
ui32Load = (SysCtlClockGet() / 25000) ;
/*PWMGenPeriodSet(PWM0_BASE, PWM_GEN_0, ui32Load);
PWMPulseWidthSet(PWM0_BASE, PWM_OUT_1, 900);
PWMOutputState(PWM0_BASE, PWM_OUT_1_BIT, true);
PWMGenEnable(PWM0_BASE, PWM_GEN_0);*/
PWMGenConfigure(PWM0_BASE, PWM_GEN_0, PWM_GEN_MODE_UP_DOWN | PWM_GEN_MODE_NO_SYNC);
PWMGenPeriodSet(PWM0_BASE, PWM_GEN_0, ui32Load);
PWMGenIntTrigEnable(PWM0_BASE, PWM_GEN_0, PWM_TR_CNT_LOAD | PWM_TR_CNT_ZERO |PWM_INT_CNT_ZERO | PWM_INT_CNT_LOAD |
PWM_INT_CNT_AU | PWM_INT_CNT_AD | PWM_INT_CNT_BU |
PWM_INT_CNT_BD | PWM_TR_CNT_ZERO |
PWM_TR_CNT_LOAD | PWM_TR_CNT_AU | PWM_TR_CNT_AD |
PWM_TR_CNT_BU | PWM_TR_CNT_BD );
PWMGenEnable(PWM0_BASE, PWM_GEN_0);
PWMPulseWidthSet(PWM0_BASE, PWM_OUT_0, 2700);
PWMOutputState(PWM0_BASE, PWM_OUT_0_BIT, true);
}
void handler_ADC(void)
{
ADCIntClear(ADC0_BASE, 1);
ADCSequenceDataGet(ADC0_BASE, 1, &ui32ADC0Value[0]);
ADCSequenceDataGet(ADC0_BASE, 1, &ui32ADC0Value[1]);
ADCSequenceDataGet(ADC0_BASE, 1, &ui32ADC0Value[2]);
ADCSequenceDataGet(ADC0_BASE, 1, &ui32ADC0Value[3]);
ADCSequenceDataGet(ADC0_BASE, 1, &ui32ADC0Value[4]);
ADCSequenceDataGet(ADC0_BASE, 1, &ui32ADC0Value[5]);
ADCSequenceDataGet(ADC0_BASE, 1, &ui32ADC0Value[6]);
ADCSequenceDataGet(ADC0_BASE, 1, &ui32ADC0Value[7]);
cnt++;
ui32ADCAvg = (ui32ADC0Value[0]+ui32ADC0Value[1]+ui32ADC0Value[2]+ui32ADC0Value[3]+ui32ADC0Value[4]+ui32ADC0Value[5]+ui32ADC0Value[6]+ui32ADC0Value[7])/8;
}