Part Number: RM48L952
Other Parts Discussed in Thread: HALCOGEN
HI,
Please clarify the below doubts on the Flash Emulated EEPROM (FEE) module.
| S.No | Device | Test identifier | Clarifications |
| 1 | Flash Emulated EEPROM (FEE) |
FEE1 | Whether SL_Init_ECCFlash need to be called? Whether ESM 1.35 and ESM 1.36 events occur if the fault is detected? |
| 2 | FEE2A, FEE2B | SL_CRC_Calculate function calculates the CRC using the internal CRC module. Is any Halcogen configuration need to be done for this test? | |
| 3 | FEE3 | Which type of ESM event will occur? | |
| 4 | FEE4 | Whether ECC protection is enabled on boot? Does any API need to be called to enable flash protection? Or is it an Halcogen configuration? | |
| 5 | FEE7 | Which type of ESM event will occur? | |
| 6 | FEE8 | Is FEE_ECC_DATA_CORR_MODE are the correct test types to perform this test? | |
| 7 | FEE9 | Is FEE_ECC_SYN_REPORT_MODE are the correct test types to perform this test? | |
| 8 | FEE10 | Is FEE_ECC_MALFUNCTION_MODE1 are the correct test types to perform this test? | |
| 9 | FEE11 | Is FEE_ECC_MALFUNCTION_MODE2 are the correct test types to perform this test? | |
| 10 | FEE12 | Writing into the emulated EEPROM using F021 flash API. | |
| 11 | FEE13 | How to perform software tests for hardware CRC? | |
| 12 | FEE14 | How to perform this test? Whether this feature is internal to RM48 MCU? |
Regards,
Monish P