Part Number: RM48L952
Hi,
Please clarify the below doubts on the Real-Time Interrupt (RTI) Operating System Timer module.
| S.No | Device | Test identifier | Clarifications |
| 1 | Real-Time Interrupt (RTI) Operating System Timer | RTI1 | One counter is used for the application and another counter is a free-running counter. So, application SW should periodically compare the counter value in both timers. If the comparison is not the same, then it is considered an error. Is our understanding correct? Whether this diagnostic functionality needs to be implemented for both RTOS and bare-metal code? |
Regards,
Monish P