This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MCU-PLUS-SDK-AM243X: EPWM cannot be output normally about the AM243x-LP

Part Number: MCU-PLUS-SDK-AM243X


Hi Experts,

    I am using the EPWM Duty Cycle example, as below:

C:\ti\mcu_plus_sdk_am243x_08_01_00_36\examples\drivers\epwm\epwm_duty_cycle

   and I know the example

  • Configures ePWM0 to generate a 1KHz signal with 25% duty cycle for 60 seconds

   So, I use the Oscilloscope to connect the Pin 1 of J2 header on am243x-lp board, but I did not see any change as below:

   I am not sure that is this example normal? and I saw that the example is indeed finished, but it reports the errors as below: