Part Number: TM4C1294KCPDT
Hi team,
Here's an issue may need your help:
Issue: now PM0, PMI in parallel, PM2, PM3 in parallel, PM4, PM5 in parallel, PM6, PM7 in parallel, as CCP input to Timer (one measured rising edge, one measured falling edge), input square wave signal on PM0.1, it's found that PM2.3 also have similar square wave signal (large amplitude), PM4.5 PM6.7 too with small amplitude. Input the square wave on PM4.5, and the same square wave signal is found on PM6.7, PM0.1, PM2.3 also has very small square wave signals.
So the customer would like to know if the PM0, 1, 2, 3 Pin internal and PM4, 5, 6, 7 pin internal has some correlation? Could you help check this case? Thanks.
Best Regards,
Cherry