Part Number: TM4C129LNCZAD
Table 31.8 on page 2067 of the microcontroller data sheet requires the LDO capacitor to have a specific ESR and LSR. At what frequency is the capacitor to have these values?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TM4C129LNCZAD
Table 31.8 on page 2067 of the microcontroller data sheet requires the LDO capacitor to have a specific ESR and LSR. At what frequency is the capacitor to have these values?
Hello John,
We don't have a specification for frequency listed because that is more system dependent. The frequency on the capacitor would be influenced by your actual hardware and if noise is impacting the capacitor etc. The same applies for accounting for the temperature range of your board. Both frequency and temperature on the capacitor will impact ESR and needs to be assessed for each design.
Our System Design Guidelines provide a bit more detail on the LDO cap, see Section 3.4.2: https://www.ti.com/lit/pdf/spma056
Essentially you want capacitors that are low ESR and have better than 10% tolerance. It is strongly recommended to use ceramic caps. Ceramics are recommended over dielectric capacitors due to the wide tolerance over temperature that dielectrics have.
Best Regards,
Ralph Jacobi
Hello Ralph,
The regulator on the chip is a linear regulator whose stability is influenced by the ESR and ESL. This link
shows on page 46 section 9.3 the conditions under which the ESR and ESL are specified as determined by the internal regulator (see note 2). Small capacitors, 0.1, 0.01 µF are effective for system noise. 2.5 to 4.0 µF are not as effective and are for lower frequencies.
I agree temperature is a factor as well as the dielectric material. You recommended ceramic capacitors over dielectric capacitors. All capacitors have dielectrics. What do you mean by dielectric capacitors?
John
Hello John,
shows on page 46 section 9.3 the conditions under which the ESR and ESL are specified as determined by the internal regulator (see note 2). Small capacitors, 0.1, 0.01 µF are effective for system noise. 2.5 to 4.0 µF are not as effective and are for lower frequencies.
That may be how ST is providing their specs based on their LDO design but we don't have such a specification for TM4C devices.
Section 3.4.2 of the System Design Guidelines discusses which capacitor values to use, you will want 3.3uF or 3.4uF depending on how you want go about add bulk and decoupling caps.
I agree temperature is a factor as well as the dielectric material. You recommended ceramic capacitors over dielectric capacitors. All capacitors have dielectrics. What do you mean by dielectric capacitors?
Sorry, it was a specific dielectric that is not recommended. "Z5U dielectric capacitors are not recommended due to wide tolerance over temperature."
Best Regards,
Ralph Jacobi
Hello Ralph,
the first paragraph is section 3.4.2 of the System Design says the voltage regulator requires a capacitor to operate properly. Nothing about system frequencies. Our system will have frequencies at 20Kh, 10 MHz and 120 MHz to name a few. It is going to be very hard to find a capacitor that has an ESR below 100 mΩ over these frequencies. If you can find one I would like to know its part number.
John
Hello John,
We have capacitors in our BOM for our LaunchPad https://www.ti.com/lit/pdf/spmu365
I had spoken with my colleague earlier and confirmed with him that this is something that is a system concern. 120MHz doesn't seem like a frequency that should be propagating through your system at all. Most customers look in the 1-10MHz range.
Best Regards,
Ralph Jacobi
Also it looks like the Filter Capacitor in particular is where the low ESR is most important as that is specifically called out in the BOM as Low ESR: