Part Number: TM4C123GH6PM
Hi Folks,
I'm creating a custom PCB and want to correctly connect the SoftSSI lines to drive a SPI device:
I have the following available:
SoftSSIClk - PA2
SoftSSIFss - PA3
SoftSSIRx - PA4
SoftSSITx - PA5
I'm figuring:
SoftSSIClk -> SPI_SCK
SoftSSIRx -> SPI_MISO
SoftSSITx -> SPI_MOSI
But I'm really not sure what to do with: SoftSSIFss what is it in terms of SPI communications? (Other than the 3 lines above, I just need chip select which I can use any GPIO for.)
thanks for any clarification!
Bob