Part Number: TM4C1294NCPDT
Hi,
What is the max serial clock that the SSI interface can work?
BR,
Barak
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TM4C1294NCPDT
Hi,
What is the max serial clock that the SSI interface can work?
BR,
Barak
Hello Barak,
It depends on the mode you are operating in.
For Master mode, the SSI clock max speed is /2 the system clock. The highest system clock is 120 MHz so the maximum SSI clock as a Master would be 60 MHz.
For Slave mode, the system clock needs to be 12x faster than the SSI clock. So at 120 MHz, the maximum SSI clock as a Slave would be 10 MHz.
Best Regards,
Ralph Jacobi