Part Number: TMS570LS1114
Other Parts Discussed in Thread: UNIFLASH
hi,The Flash ECC diagnosis function has the following questions,Also hope to reply as soon as possible, thank you.
(1) The diagnostic function of Flash in my project uses ECC, so when the generated target file is burned to Flash, the corresponding ECC check code needs to be burned to the corresponding address, the code address starts at 0x00000, and the corresponding ECC check code starts at 0xF0400000, as shown in the figure below, is that right?


(2) The burning tool uses uniFlash, so can the ECC check code corresponding to the burning file be enabled as follows? Is it to burn the ECC verification code to the address 0xF0400000, because I did not see the setting options for the ECC verification code burn address, can I just check the following?