Part Number: TM4C1294NCPDT
Other Parts Discussed in Thread: EK-TM4C1294XL
I am working on EK-TM4C1294XL. I am not able to get any data from PA1_CAN0TX pin. Anything wrong in my code? my code as below:-
void CAN0_Init(void)
{
pui8MsgData = (uint8_t *)&ui32MsgData;
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
GPIOPinConfigure(GPIO_PA0_CAN0RX);
GPIOPinConfigure(GPIO_PA1_CAN0TX);
GPIOPinTypeCAN(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
SysCtlPeripheralEnable(SYSCTL_PERIPH_CAN0);
CANInit(CAN0_BASE);
// uint32_t ui32SysClock;
// ui32SysClock = SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ |SYSCTL_OSC_MAIN |SYSCTL_USE_OSC)25000000);
// CANBitRateSet(CAN0_BASE, ui32SysClock, 500000);
/////////////////
SysCtlClockSet(SYSCTL_SYSDIV_1 | SYSCTL_USE_OSC | SYSCTL_OSC_MAIN |SYSCTL_XTAL_16MHZ);
CANBitRateSet(CAN0_BASE, SysCtlClockGet(), 500000);
CANIntEnable(CAN0_BASE, CAN_INT_MASTER | CAN_INT_ERROR | CAN_INT_STATUS);
IntEnable(INT_CAN0);
CANEnable(CAN0_BASE);
ui32MsgData = 0;
sCANMessage.ui32MsgID = 1;
sCANMessage.ui32MsgIDMask = 0;
sCANMessage.ui32Flags = MSG_OBJ_TX_INT_ENABLE;
sCANMessage.ui32MsgLen = sizeof(pui8MsgData);
sCANMessage.pui8MsgData = pui8MsgData;
}
//____________________________________________________________________
void CAN0_Send(void)
{
CANMessageSet(CAN0_BASE, 1, &sCANMessage, MSG_OBJ_TYPE_TX);
// SimpleDelay();
// ui32MsgData++;
ui32MsgData=0xaa;
}