This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RM48L952: CC no longer builds project, Gmake error 2

Part Number: RM48L952
Other Parts Discussed in Thread: HALCOGEN

Code composer v11.0.0.00012

Descr:  Previously building Micrium project no longer builds. 

This problem started recently after a new workspace and second instance of this project was created. 

The errors I see during build are "error 2" from gmake.  I know this indicates possible mispelling of path or other.

I do see a non-existing include path, but I have not found where it gets into the project.  Maybe it comes from Halcogen somehow.

Is there a way to increase the verbosity, or inspect the opt files ?  Or some *.ccxml file ? That would really help me troubleshoot.

I am tempted to write a dos/windows program and name it armcl.exe to at least see what values are being passed to the compiler.

VISIBILITY is what I need please.