Part Number: TM4C1294NCPDT
Other Parts Discussed in Thread: SYSBIOS
Based on setup
* : CCS 11.0 Or latest version.
* : Complier TI x20.2.6.LTS Or latest version.
* : XDCTools 3.32.2.25
* : TI-RTOS for TivaC <tirtos_tivac_2_16_01_14>
* : TivaWare_C_Series 2.1.1.71b
I wish to check heap from time to time temporary during runtime and then remove it.
I have reviewed the SPRUEX3P, page 166 mentioned about HeapTrack and
file:///E:/010_WorkAOT/011MyGit20/106-TM4C_2021/tirtos_tivac_2_16_01_14/products/bios_6_45_02_31/docs/cdoc/ti/sysbios/heaps/HeapTrack.html
I placed the code in cfg
/* ================ Kernel (SYS/BIOS) configuration ================ */
var BIOS = xdc.useModule('ti.sysbios.BIOS');
//BIOS.assertsEnabled = true;
BIOS.assertsEnabled = false;
/*
* Specify default heap size for BIOS.
*/
//BIOS.heapSize = 5120; //ex 1024. 5120 for FATFS.
BIOS.heapSize = 10000; //Will it fix crashes?
BIOS.heapTrackEnabled = true; // RGP: 6Jan21: To debug Heap operation ,remove when not needed.
BIOS.includeXdcRuntime = false;
//BIOS.includeXdcRuntime = true;......
//----------------------------------------------Heap Debug
#include <ti/sysbios/heaps/HeapTrack.h> // to debug heaps. See SPRUEX3T, page 166.
#include <xdc/runtime/IHeap.h>
#include <xdc/runtime/Memory.h>
......
HeapTrack_Handle heap;
void RFD_Heap_Init(void)
{
//-------------------------Heap Monitor
HeapTrack_Params prms;
//HeapTrack_Handle heap;
Error_Block eb;
Error_init(&eb);
HeapTrack_Params_init(&prms);
prms.heap = heapHandle;
heap = HeapTrack_create(&prms, &eb);
if (heap == NULL) {
System_abort("HeapTrack create failed");
}
}
I'm not sure where "heapHandle" come from?, can u advise?
Thanks.