Part Number: LAUNCHXL2-RM57L
Other Parts Discussed in Thread: HALCOGEN
I tried to remove MISRA-C warning in SCI Module. I enabled SCI1 in halcogen and generated the code
Please check CCS will support following solution or not
Warning : Array Indexing is the only allowed form of pointer arithmetic
void sciSend(sciBASE_t *sci , uint32 length , uint8 *data)
{
while(length > 0U)
{
while((sci->FLR & (uint32)SCI_TX_INT)==0U)
{
}
txdata = *data;
sci -> TD = (uint32)( txdata );
data++;
length--;
}
}
In the above programme, "data" is the pointer variable, which stores the address, we should not increment the pointer variable according to Misra C rule. Hence, By giving the array as the parameter to function, we can access through array indexing.
void sciSend(sciBASE_t *sci, uint32 length, uint8 data[ ])
{
while(length >0)
{
uint8 count;
while ((sci->FLR & (uint32)SCI_TX_INT) ==0U)
{
}
txdata = data[count];
sci -> TD = (uint32)(txdata);
count++;
length--;
}
}