Part Number: RM57L843
Hi team,
Here's some issues from the customer may need your help:
The related thread has been created as above.
a. The ESM has only one nError output pin, and if there are multiple errors at the same time, how to determine which one is wrong? Is it necessary to test which part of the problem with the API of each module of the diagnostic library at this time?
b. Also, for correctable 1-bit ECC errors, is it fixed automatically or is it corrected by calling its corresponding diagnostic API?
c. Regarding the return value of the diagnostic API (TRUE/FALSE), dose it mean whether the test is successful, or jus indicate here's something wrong?
Could you help check this case? Thanks.
Best Regards,
Cherry