Part Number: UNIFLASH
Other Parts Discussed in Thread: CCSTUDIO
I am trying to install Uniflash and have been receiving errors using both the web and offline installation links. I am running a Windows 11 machine (emulating Windows 11 on an ARM Macbook M1) and have CCS 9.3.0 (I need this version specifically) installed. I'm not sure if I'm missing anything else that needs to be installed. Anything helps, thanks.
Using the offline installer, I get the following error: "file:///Mac/Home/Downloads/uniflash_3.4.1.00012_win32/Uniflash_3.4.1.00012_win32/repo" -installiu com.ti.ccstudio.p2tool.install.feature.group -destination "C:\ti\uniflash_3.4/eclipse" -nosplash: org.eclipse.equinox.p2.core.ProvisionException: Error: file:///Mac/Home/Downloads/uniflash_3.4.1.00012_win32/Uniflash_3.4.1.00012_win32/repo is not a valid extension location because it already contains a standard p2 repository file."
Screenshot shows the error I see when installing from the web version. If it helps, I am only looking for support on 32xx controllers (I only selected that type during install).