Part Number: TMS570LS3137
Hello,
I have a question regarding the interrupt handling:
I would like to only disable a specific interrupt ttemporarily e.g. rti compare 0 during the execution of a function which is happening in a background loop e.g. main method.
Are there some alternatives how to proceed with that issue?
Should I use VIM register to mask out that specific interrupt or can I easily use the ClearInt Register of the RTI interface to disable the corresponding interrupt line temporarily till my function has executed to enable it again afterwards ?
I mean globally I could easily disable all interrupts during this function context but this is something I would like to avoid.
It is also important that you dont't miss any pending interrupt from this interface as the interrupt IRQ line still remains essential for the applicaiton.
It should just "sleep" while cricital code sections are executed. Once this critical code section is left, in case any pending interrupt from the masked IRQ is available it should fire the coressponding IRQ line.
I have read the document for nested interrupts on the Hercules platform but this document specifies more the handling during pure interrupt context execution.
Is there something I can reuse or simplifiy in order to achieve the behavior described above ?