Part Number: LP-AM243
Other Parts Discussed in Thread: SYSCONFIG
Using the standard LP-AM243 for an application .
Can the serial port support 2 M of baud
Can you please send me a screen capture of the setup for 2 M baud eg. below

Thanks
Dinesh
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Dinesh,
The UART documentation mentions the driver is currently contrained to UART 16x mode (<= 115.2 Kbaud/s), please see: https://software-dl.ti.com/mcu-plus-sdk/esd/AM243X/08_01_00_36/exports/docs/api_guide_am243x/DRIVERS_UART_PAGE.html
Nevertheless, the Sysconfig parameters for the UART can be set for 2 Mbaud as follows:
The UART hardware supports three modes of operation, please see the AM64x/AM243x TRM (spruim2c.pdf), 12.1.5.2.1.3 UART Protocol and Data Format.
For 2 Mbaud, the mode must be set to 13x oversampling.
It should be possible to select a 192/96/64/48 MHz or 160 MHz UART functional clock (FCLK). Please see TRM:
FCLK is further divided by the UART Divisor (DLH:DLL registers).
The final baud rate will be FCLK/Divisor/13, which may not be exactly 2 Mbaud, i.e. there will be some error in the baud rate.
I'm able to change FCLK supplied to the UART by changing the Sysconfig setting for "Clock Freq", but the UART driver internal clock is fixed at 48 MHz. I need to review this with the software development team to see if I'm missing something. I'll keep you posted.
Regards,
Frank
Hi Dinesh,
Please see the following in the TRM for additional information about the UART baud rate:
Notice the UART supports up to 3.6884 Mbps in 13x mode with a 48 MHz functional clock.
Regards,
Frank
Dinesh,
The UART driver documentation is incorrect ("UART 16x mode (<= 115.2 Kbaud/s)"), and 13x mode is supported.
Regards,
Frank
Dinesh,
We're still investigating the issue with fixed 48 MHz UART functional clock, but this shouldn't prevent you from configuring the UART baud rate using Sysconfig as I've outlined above. Hence, I'll close this thread.
Regards,
Frank