Part Number: TM4C1294NCPDT
I have created a TCP client based on TCP echo example for TN4C1294NCPDT,but server connection failed
client code-
Void tcpHandler(UArg arg0, UArg arg1)
{
int sockfd;
struct sockaddr_in servaddr;
while(1)
{
// socket create and varification
sockfd = socket(AF_INET, SOCK_STREAM, IPPROTO_TCP);
if (sockfd == -1) {
printf("socket creation failed...\n");
exit(0);
}
else
printf("Socket successfully created..\n");
memset(&servaddr, 0, sizeof(servaddr));
// assign IP, PORT
servaddr.sin_family = AF_INET;
servaddr.sin_addr.s_addr = inet_addr("192.168.1.4");
servaddr.sin_port = htons(PORT);
// connect the client socket to server socket
if (connect(sockfd, (SA*)&servaddr, sizeof(servaddr)) != 0){
printf("connection with the server failed...\n");
// exit(0);
}
else
printf("connected to the server..\n");
}