This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
Here's an issue from the customer may need your help:
After downloading and installing diagnostic library, the demo program can be compiled or downloaded to the board. But the program doesn't work, the board doesn't react, and the customer tried to print the information in the serial port and control the LED light in the IO port, but both failed.
Could you help check what's the reason for that? Thanks.
Best Regards,
Cherry
Hi,
1. Does your customer use TI launchpad or TI HDK?
They use the development board of LAUNCHXL2-RM57L.
2. When they load the program to the flash, is "ECC Auto Generate" enabled?
Regarding this, program is downloaded from here. And the customer don't know whether the ECC Auto Generate is enabled and no other additional resources are being used on the development board.
Thanks and regards,
Cherry
Hi Cherry,
"Auto ECC Generation" is an option when loading the program to the flash.
CCS-->Tools --> On-Chip Flash
Hi,
Thanks!
They have checked and the "Auto ECC Generation" is enabled.
Thanks and regards,
Cherry
Hi Cherry,
Is the nERROR LED (LED1, at left-bottom corner) turned ON? The code will get stuck in the while(1) loop (in start_up.c) if any severe error:
Hi Wang,
Is the nERROR LED (LED1, at left-bottom corner) turned ON? The code will get stuck in the while(1) loop (in start_up.c) if any severe error:
Is nERROR configured in halcodegenerator?
Thanks and regards,
Cherry
Hi,
May I know is there any updates regarding the additional question?
Thanks and regards,
Cherry
Hi Cherry,
Is nERROR configured in halcodegenerator?
The ESM Group1 errors have a configurable interrupt response and configurable ERROR pin behavior. those can be configured in HALCOGen.
But ESM Group 2 and Group 3 errors always generate an output on the ERROR pin.