Other Parts Discussed in Thread: UNIFLASH, , CC1350
Hello team e2e,
I am trying to use the msp432e401y launchpad as mentioned in the user guide using uniflash (section 7.2) -> https://www.ti.com/lit/ug/sluuc29b/sluuc29b.pdf?ts=1642509312710&ref_url=https%253A%252F%252Fwww.ti.com%252Ftool%252FTPS92520EVM-074, but unfortunately I see the following error. My jumper settings on microcontroller are also shown -->



After this I also tried to run one example LED code on CCS, and I see the following error (more or less the same as in uniflash) -->
Error initializing emulator: (Error -260 @ 0x0) An attempt to connect to the XDS110 failed. The cause may be one or more of: no XDS110 is connected, invalid firmware update, invalid XDS110 serial number, or faulty USB cable. The firmware and serial number may be updated using the xdsdfu utility found in the .../ccs_base/common/uscif/xds110 directory of your installation. View the XDS110SupportReadMe.pdf file there for instructions. (Emulation package 9.5.0.00143)

PS. I tried using 2-3 different USB cables already and still the problem persists. However, I ran one example LED code with cc1350 launchpad and that works in one go.
Could you please assist me in figuring out the possible source of error here ?
Thank you,
Anubha