Part Number: TMS570LC4357
Other Parts Discussed in Thread: HALCOGEN
Hi Ti Team/ QJ Wang,
I have issue in size of bin if i use Flash1 (Bank 1) memory for the project or build.
Post-build steps
"${CCS_INSTALL_ROOT}/utils/tiobj2bin/tiobj2bin" "${BuildArtifactFileName}" "${BuildArtifactFileBaseName}.bin" "${CG_TOOL_ROOT}/bin/armofd" "${CG_TOOL_ROOT}/bin/armhex" "${CCS_INSTALL_ROOT}/utils/tiobj2bin/mkhex4bin"

VECTORS (X) : origin=0x00000000 length=0x00000020
FLASH0 (RX) : origin=0x00000020 length=0x001FFFE0
FLASH1 (RX) : origin=0x00200000 length=0x00200000
STACKS (RW) : origin=0x08000000 length=0x00001500
RAM (RW) : origin=0x08001500 length=0x0007EB00
bin file size is 62k for LED blink , FEE and CAN.
same build with
VECTORS (X) : origin=0x00200020 length=0x00000020
FLASH0 (RX) : origin=0x00000020 length=0x001FFFE0
FLASH1 (RX) : origin=0x00200040 length=0x001FFFBF
STACKS (RW) : origin=0x08000000 length=0x00001500
RAM (RW) : origin=0x08001500 length=0x0007EB00
Bin file size is 2049k for same project
LED blink , FEE and CAN functionality.
Please explain the
Thanks in Advance.
Santhosh