Part Number: AM2434
Other Parts Discussed in Thread: SYSCONFIG
Hello,
is there an example for the TMDS243GPEVM that illustrates how to use the PRU ICSSG PWM module?
From the AM243x TRM I gather that the PWM outputs are affected by compare matches between between IEP_COUNT_REGx and IEP_CMPy_REGz. From section 6.4.10.2 I gather that a CMPx event sets the output x (active state) and a CMP0 event resets the output (initial state). Is that correct? So all ICSSG PWM outputs can enter active state at different times (according to their CMP registers) but enter initial state all at the same time corresponding to CMP0?
Where can I find more information on the PRU ICSSG PWM module? I am having difficulties to understand it based on the information provided in the TRM.
Where do I find the PRU ICSSG PWM outputs in sysconfig?
Can PRU ICSSG PWM generation be used together with industrial internet or EnDat functionality?
Best regards,
Johannes