This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RM48L952: EMIF_Interface

Part Number: RM48L952

Hi We are using Ethernet 16 bit parallel bus controller  using RM48 device.

Here i want to know about What is the Enable EMIF Asycnc1,EMIF Asycnc 2, EMIF Asycnc 3 what is the purpose of this which one need to configure for our operation.

Please help us to solve this issue.

Thanks and Regards,

Ganesh V

  • Hi Ganesh,

    RM48 EMIF module has four chip selects: CS0, CS2, CS3, CS4. CS0 is used to select a synch memory device, but CS2/3/4 are used to select a async memory device.

    If you want to use the Ethernet controller as a EMIF Async, you can use either CS2, or CS3, or CS4. I used CS2 for one Ethernet Controller before.