Part Number: AM2732
Other Parts Discussed in Thread: TMS320C6747
Hi experts,
My customer is considering the AM2732 for audio products that will be mass produced in 2023 or later.
Q1:Will the AM2732 be the most suitable successor to the TMS320C6747 (400MHz)? Please let me know if there are any other products in the AM27xx series that will be RTM'd in the future that would be optimal.
Q2:When I want to use McASP of AM2732, it is pin muxed, but there is no DataSheet for signal timing, etc. Can I actually use it?
Q3:Since there is no I/F for external memory such as EMIF, is it correct to recognize that QSPI is a place to store programs and basically run applications using only internal RAM? Is it assumed that only internal RAM is used?
Q4:I think it is difficult to evaluate Audio with TMDS273GPEVM, but is there any other EVM that can evaluate Audio?
Q5:Could you tell me if there are any precautions to be taken when migrating Audio applications from TMS320C6747 to AM2732?
Best regards,
O.H