This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LC4357: Sync Frame/Startup

Part Number: TMS570LC4357

Hello,

I have just 2 TMS5704357 Launch eval boards connected together in a Flexray network on Flexray 1 connections.

The SUCC1 register is set to 0x0F1FFB00, which configures the chip for:

 Ch A & B enabled, MTS Tx on A & B, Sync frame, and startup frame.

This the original config value that was in the code from TMS570LS3137_FlexRay_Example. 

In FlexRay.h the definition of NODE_TOTAL = 25 and SYNC_NODE = 8.

Should NODE_TOTAL and SYNC_NODE be changed to 2 ??

Thank you,

David