Part Number: AM2431
Hi,
My customer is now considering AM243x and some questions about M4F. Could you answer some their questions below ?
Can M4F on AM2431 execute the code on DDR4 ?
MCU domain is isolated from SoC on the Safety option F device, correct ?
On the safety-capable device (F option), M4F cannot access the peripherals in MAIN domain ?
MCU_CBASS0 interconnect in MCU domain is not connected to CBASS0 in MAIN domain ?
Can M4F on AM2431 which doesn’t have F option access peripherals in MAIN domain such like DDR, PCIe, GPIO, etc… ? Can it access directly to the memory mapped registers of peripherals in MAIN domain ?
Are the both frequency of CBASS0 and MCU_CBASS0 250MHz ? What are the bus width (bit) of CBASS0 and MCU_CBASS0 ?
Regards,
Hideaki