Part Number: RM48L952
Hi Ti,
A. Whether for the following tests, the nError trigger will occur. Because when we tested the below diagnostics, we observed nError trigger.
- SL_SelfTest_Flash - FLASH_ECC_ADDR_TAG_REG_MODE
- SL_SelfTest_Flash - FLASH_ECC_TEST_MODE_2BIT
- SL_SelfTest_Flash - FLASH_ADDRESS_ECC_SELF_TEST
- SL_SelfTest_SRAM - SRAM_ECC_ERROR_FORCING_2BIT
- SL_SelfTest_SRAM - SRAM_RADECODE_DIAGNOSTICS
- SL_SelfTest_VIM - VIM_SOFTWARE_TEST);
B. Also after the DCAN - Parity test using SL_SelfTest_CAN(CAN_SRAM_PARITY_TEST, SL_DCAN1), we tested the CAN interface functionality. We observed ESM Group 1 and Channel 21 callback error occurs continuously. Is there any way to solve this problem?
C. For ADC input pin testing using function SL_SelfTest_ADC(ADC_SELFTEST_ALL, 0U, &adc_config, &pinStatus), we observed ADC_CH0 failure. What is the cause of the failure?
Regards,
Monish P