Part Number: RM57L843
Hi team,
Here's some issues from the customer may need your help:
The Diagnostic Library API is only used to test if a module has the ability to error-check (ECC), and it is not possible to detect if a module (such as memory) has made an error while a program is running. Is that right?
For example, SL_SelfTest_CAN() is an API that does not detect if there is a problem with the CAN's internal program operation, but can only test whether it has the ability to correct errors by simulating a 1- or 2-bit error injection?
If so, will the error generated by the analogue test trigger a level change on the nERROR pin?
Could you help check this case? Thanks.
Best Regards,
Cherry