Part Number: TMS570LC4357
Hello,
I am using the 6837.TMS570LS3137_FlexRay_Example code provided by TI. I have only 2 nodes on the network. I am monitoring the bus traffic
with a logic analyzer. The two nodes are alternating transmitting messages on the bus as they should. However, neither node detects the "new data" flags when executing the
transmit_check_node function. Consequently, the Fr_ReceiveRxLPdu function is not called, so no data is received from the other node.
I have made some changes to get the bus started and running (clocks, ETC), but have not made any changes re: buffer configuration. That is unchanged from the
original example code.
Any insight you can provide would be much appreciated.
Thank you,
David