Part Number: AM2434
Other Parts Discussed in Thread: SYSCONFIG
Extending the epwm_duty_cycle.c example from mcu_plus_sdk_am243x_08_01_00_36 I have added code to start the ADC (by EPWM SOCA and SOCB) and an ISR to read out ADC values. This appears to work fine as long as I don't use DebugP_log() in
while(numIsrCnt > 0)
{
char buf[256];
SemaphoreP_pend(&gEpwmSyncSemObject, SystemP_WAIT_FOREVER);
if (isr_data.f != 0) {
snprintf(buf, sizeof(buf), "%2d kHz, ADCH_0: %4d, ADCH_1: %4d %d %d\n",
isr_data.f, isr_data.ADC_step0_data, isr_data.ADC_step1_data, isr_data.sync_isr_cnt, isr_data.adc_isr_cnt);
// DebugP_log(buf); // uncommenting this stops the ADC interrupt after a short time
isr_data.f = 0;
}
numIsrCnt--;
}
at the end of epwm_duty_cycle_main().
I have changed interrupt priorities in the structs passed to HwiP_construct() and in SysConfig's Debug Log section but have had no success. As soon as I call DebugP_log() the ADC ISR is stopped being called after a short time.
The ADC ISR looks like this:
void App_adcISR(void *handle)
{
uint32_t fifoData;
uint16_t t_entry = SyncEpwm->TBCTR;
GPIO_pinWriteHigh(gpioBaseAddr, GPIO32_PIN);
SOC_controlModuleUnlockMMR(SOC_DOMAIN_ID_MAIN, 1);
pMainMmrCtrl->ADC0_CTRL ^= 1; // toggle between EPWM_SOCA_OUT and EPWM_SOCB_OUT
SOC_controlModuleLockMMR(SOC_DOMAIN_ID_MAIN, 1); // doesn't work, lock code is disabled by #if 0
if (t_entry > entry_max_adc) entry_max_adc = t_entry;
if (t_entry < entry_min_adc) entry_min_adc = t_entry;
adc_isr_cnt++;
/* Get interrupt status and clear */
adcstatus = ADCGetIntrStatus(ADC0baseAddr);
fifo_cnt = ADCGetFIFOWordCount(ADC0baseAddr, ADC_FIFO_NUM_0);
fifoData = ADCGetFIFOData(ADC0baseAddr, ADC_FIFO_NUM_0);
ADC_step0_id = ((fifoData & ADC_FIFODATA_ADCCHNLID_MASK) >> ADC_FIFODATA_ADCCHNLID_SHIFT);
ADC_step0_data = ((fifoData & ADC_FIFODATA_ADCDATA_MASK) >> ADC_FIFODATA_ADCDATA_SHIFT);
fifoData = ADCGetFIFOData(ADC0baseAddr, ADC_FIFO_NUM_0);
ADC_step1_id = ((fifoData & ADC_FIFODATA_ADCCHNLID_MASK) >> ADC_FIFODATA_ADCCHNLID_SHIFT);
ADC_step1_data = ((fifoData & ADC_FIFODATA_ADCDATA_MASK) >> ADC_FIFODATA_ADCDATA_SHIFT);
ADCClearIntrStatus(ADC0baseAddr, adcstatus);
GPIO_pinWriteLow(gpioBaseAddr, GPIO32_PIN);
/* Set EOI to generate next interrupt if any */
ADCWriteEOI(ADC0baseAddr);
}
My question is: What is the best way to get debugging output on the console?
Best regards, Johannes