Part Number: TMS570LC4357
Hi Experts,
I have a question regarding the use of ECLK1(A12) and ECLK2 (K3) as GIO:
If I understand this correctly the pin K3 can me muxed to ECLK2 and ECLK2 can then be configured as a GIO, while the pin A12 is always ECLK1, which can also be used as GIO.
According to the Datasheet the Configuration of ECLK (I would assume this to be ECLK1) to GIO can be done in register SYSPC1 to SYSPC2.
(Q1) Since that ssems to be the way to control ECLK1 as GIO, how can ECLK2 be configured as GIO and how is it controlled?
Thank you and best regards,
Max