This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP432E401Y: Dynamic setting of conflict pins using Sysconfig.

Guru 12885 points
Part Number: MSP432E401Y
Other Parts Discussed in Thread: SYSCONFIG,

Hi,

Each pin is set using Sysconfig.

 

[Question 1]
I want to dynamically switch functions using the same pin.

Specifically, I want to use the RX pin of the UART as the input interrupt pin of GPIO, and when an input interrupt comes, I want to wake up the CPU and switch to the UART for communication.

Sysconfig is a GUI-based tool for initial pin settings.

Therefore, when dynamically switching pin assignments as described above, it is necessary to describe in the code base without using sysconfig . Is this my understanding correct?

 

[Question 2]
If Question 1 is "Yes", how should I write the interrupt handler on the side that is not registered on Sysconfig?

If you registered with Sysconfig, you can set it with GPIO_setCallback.

However, in the case of conflicting pins, GPIO_setCallback cannot be used because it cannot be registered with Sysconfig?

I feel that it can be done by using "Hwi_create", but there are some places where I don't know how to use it, so I would like advice such as the best solution.


Device: MSP432P401R

OS: TI-RTOS

Thanks,

Koki