This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SIMPLELINK-MSP432-SDK: LWIP 1.4.1 Port

Part Number: SIMPLELINK-MSP432-SDK

Hi

I'm having an issue porting the latest version of LWIP (2.1.2) to the TM4C129 (bear with me I realise this forum is for the MSP432).

https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/1074987/tm4c129encpdt-lwip-2-1-2-port---static-ip-acquisition-mode

The Tivaware SDK only comes with version 1.4.1. I see that the Simplelink SDK includes version 2.0.2, the oldest version of which I can obtain is version 2.20.00.00.20, which also has LwIP 2.0.2 included. I wondered if there was an older version that include LwIP version 1.4.1? If there is, could you provide me with access please? I think that my issue is with either lwiplib.c or more likely tiva-tm4c129.c. Since the approach seems to be consistent across TI devices I'm hoping that doing a comparrison between 1.4.1 and 2.0.2 ports will highlight my issue.

Thanks,

HL