Part Number: EK-TM4C1294XL
Hello,
I've found an interesting behavior, and I'm wondering if anyone has an explanation for it.
I've been developing some I2C code on my EK-TM4C1294XL, and I have it mostly up and running. One weird behavior I noticed is that the I2C module doesn't generate any interrupts unless the loopback is enabled. When it's disabled, no interrupts are generated.
In both situations, I do not have the EK-TM4C1294XL connected to any external I2C devices. But I would still expect to get a start or stop interrupt, even if nothing is connected. Anybody know what's going on?
Here's some code to replicate the issue.
/**
* main.c
*/
#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_memmap.h"
#include "inc/hw_ints.h"
#include "driverlib/rom_map.h"
#include "driverlib/rom.h"
#include "driverlib/pin_map.h"
#include "driverlib/sysctl.h"
#include "driverlib/gpio.h"
#include "driverlib/i2c.h"
#include "driverlib/interrupt.h"
uint32_t g_ui32SysClock;
static bool bInterruptPending;
void I2C_Int_Handler(void)
{
uint32_t ui32IntStatus;
ui32IntStatus = MAP_I2CMasterIntStatusEx(I2C2_BASE, true);
MAP_I2CMasterIntClearEx(I2C2_BASE, ui32IntStatus);
bInterruptPending = false;
}
int main(void)
{
g_ui32SysClock = MAP_SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ | SYSCTL_OSC_MAIN | SYSCTL_USE_PLL | SYSCTL_CFG_VCO_480), 120000000);
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOL);
while(!MAP_SysCtlPeripheralReady(SYSCTL_PERIPH_GPIOL));
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_I2C2);
while(!MAP_SysCtlPeripheralReady(SYSCTL_PERIPH_I2C2));
MAP_GPIOPinConfigure(GPIO_PL0_I2C2SDA);
MAP_GPIOPinConfigure(GPIO_PL1_I2C2SCL);
MAP_GPIOPinTypeI2C(GPIO_PORTL_BASE, GPIO_PIN_0);
MAP_GPIOPinTypeI2CSCL(GPIO_PORTL_BASE, GPIO_PIN_1);
MAP_I2CMasterInitExpClk(I2C2_BASE, g_ui32SysClock, false);
MAP_I2CMasterIntEnableEx(I2C2_BASE, 0xFFF);
I2CIntRegister(I2C2_BASE, I2C_Int_Handler);
MAP_IntEnable(INT_I2C2);
//if I2CLoopbackEnable is removed, the program hangs on while(bInterruptPending)
//if I2CLoopbackEnable is kept, the program exits normally
I2CLoopbackEnable(I2C2_BASE);
MAP_I2CMasterSlaveAddrSet(I2C2_BASE, 0x03, false);
bInterruptPending = true;
MAP_I2CMasterControl(I2C2_BASE, I2C_MASTER_CMD_QUICK_COMMAND);
while(bInterruptPending);
return 0;
}