Part Number: LP-AM243
Other Parts Discussed in Thread: UNIFLASH
I ran some tests with the default UART and sent 200 characters and received them on my Visual Studios serial port listener, however when I use the following code to build a buffer (not using the strcpy method from the example), the UART sends a seemingly random lower amount of characters. In this code it should send at least 200 characters with a value of 1 but instead it sends 105. If I change trans.count to 1024 it sends 252.
The system config is the exact same as the UART echo example. I will also attach my VS code for the listener but my previous paragraph should demonstrate its probably not VSCode.
// Copy Stream to the UART Buffer
for(i = 0; i < 1024; i++) {
gUartBuffer[i] = (uint8_t)1;
}
// Send UART Stream
UART_Transaction_init(&trans);
trans.buf = &gUartBuffer[0U];
trans.count = (size_t)200;
transferOK = UART_write(gUartHandle[CONFIG_UART_CONSOLE], &trans);
APP_UART_ASSERT_ON_FAILURE(transferOK, trans);
std::cout << "COM Listener\n";
int ch = 0;
char buffer[1];
/* ... */
// Open serial port
HANDLE serialHandle;
serialHandle = CreateFile(L"\\\\.\\COM6", GENERIC_READ | GENERIC_WRITE, 0, 0, OPEN_EXISTING, FILE_ATTRIBUTE_NORMAL, 0);
// Do some basic settings
DCB serialParams = { 0 };
serialParams.DCBlength = sizeof(serialParams);
GetCommState(serialHandle, &serialParams);
serialParams.BaudRate = 115200;
serialParams.ByteSize = 8;
serialParams.StopBits = ONESTOPBIT;
serialParams.Parity = NOPARITY;
SetCommState(serialHandle, &serialParams);
// Set timeouts
COMMTIMEOUTS timeout = { 0 };
DWORD read, written;
HANDLE keyboard = GetStdHandle(STD_INPUT_HANDLE);
HANDLE screen = GetStdHandle(STD_OUTPUT_HANDLE);
timeout.ReadIntervalTimeout = 50;
timeout.ReadTotalTimeoutConstant = 50;
timeout.ReadTotalTimeoutMultiplier = 50;
timeout.WriteTotalTimeoutConstant = 50;
timeout.WriteTotalTimeoutMultiplier = 10;
SetCommTimeouts(serialHandle, &timeout);
// basic terminal loop:
do {
ReadFile(serialHandle, buffer, sizeof(buffer), &read, NULL);
WriteFile(screen, buffer, read, &written, NULL);
} while (streaming != -1);
CloseHandle(serialHandle);