Part Number: TM4C1230D5PM
I was able to create a ccxml file that powers the target through the XDS110. When editing the ccxml file, I select test connection and it works.
I save the file then try to do Run Connect Target. The error i get states the my 3.3V was not detected (because the probe didn't turn it on.)
The ccxml file under targetConfigs is marked as [Active]
I don't see what I'm doing wrong