Part Number: TMS570LC4357
Hello together,
so we are currently running into the following problem:
After we activated the VIM Interrupt Source Channel 20, which is for ESM low-level Interrupts, we are running in the "CCM-R5F - CPU compare error" flag set, which than asserts according to the manual the "CCM-R5F - self-test" flag.
To find the source of the exception we started the system with the debugger connected and stepped through each line of code. One thing we found was that, if we start-up the system with the debugger connected and step through each line of code, the compare error flag does not signal a mismatch and the system works as expected. Only when the system starts running without the debugger interferring, the compare error flag shows up.
Does somebody know if there is a way to find out which compared output signal (Global signals, interrupt signals, L1 cache interface signals, ...) did fail or has another clue which might help?
Thanks in advance and best regards,
Alex