This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LS1224: Connect W25Q128JV external EEPROM to TMS570LS1224

Genius 9880 points

Part Number: TMS570LS1224
Other Parts Discussed in Thread: HALCOGEN

Hi,

Customer want to  connect W25Q128JV external EEPROM to TMS570LS1224, please see details below.

"Hello, I want to connect W25Q128JV external EEPROM to TMS570LS1224. i am using MibSPI3 for SPI communication. In Halcogen in MibSPi3 tab i have enabled master mode, set baudrate, charlength is set to 8 . In data Transfer tab i have selected CS0 and word length is set to 3. I am able to generate 24 bit word but after connecting to EEPROm i am not getting expected values. Below is the code i am using

/** @file sys_main.c
* @brief Application main file
* @date 11-Dec-2018
* @version 04.07.01
*
* This file contains the program to successfully run 24 bit SPI Data for ADC or DAC,
*
*/

/*
* Copyright (C) 2009-2018 Texas Instruments Incorporated - www.ti.com
*
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the
* distribution.
*
* Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
* "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
* LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
* A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
* OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
* SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
* LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
* DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
* THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
* (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
* OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*
*/


/* USER CODE BEGIN (0) */
#include "system.h"
#include "mibspi.h"
/* USER CODE END */

/* Include Files */

#include "sys_common.h"

/* USER CODE BEGIN (1) */
/* USER CODE END */

/** @fn void main(void)
* @brief Application main function
* @note This function is empty by default.
*
* This function is called after startup.
* The user can use this function to implement the application.
*/

/* USER CODE BEGIN (2) */
uint32 data1=0x05;
//uint32 data2=0x06;

uint32 txdata[6]={0};
uint32 rxdata[10];

/* USER CODE END */

int main(void)
{
/* USER CODE BEGIN (3) */

txdata[2]=data1 & 0x00FF;

txdata[1]=data1>>8 & 0x00FF;
txdata[0]=data1>>16 & 0x00FF;

txdata[2]=txdata[2]<<8;

mibspiInit();


mibspiSetData(mibspiREG3,0,txdata[2]);

mibspiTransfer(mibspiREG3,0);

while((mibspiIsTransferComplete(mibspiREG3,0)==FALSE));

mibspiGetData(mibspiREG3,0,rxdata);
/* USER CODE END */



while(1);
}


/* USER CODE BEGIN (4) */

/* USER CODE END */

"

Thank you in advance.

Regards,
Maynard

  • Hi Maynard,

    Can you read the device ID?

    uint8_t txdata[6];  //48 bits for read ID

    uint8_t rxdata[6];  //48 bits for read ID

    txdata[0] = 0x90;

    txdata[1] = 0x0; //addr

    txdata[2] = 0x0;  //addr

    txdata[3] = 0x0;  //addr

    txdata[4] = 0x0; //dummy

    txdata[5] = 0x0; //dummy

  • Hi QJ,

    According to customer, they were not able to read device ID, all they get is 0xFF in rxdata

    Regards,
    Maynard

  • Hi Maynard,

    From the diagram (from EEPROM datasheet) in my last post, the CS signal keeps LOW between two transfers, so in MCU side, the CS should be configured as "CS HOLD". 

    Please check the CS setup time and hold time of W25Q128JV, then change the tC2TDELAY and tT2CDELAY to meet their requirements.

    The TMS570 supports 4 SPI clock modes (Polarity, and phase), please use a right one required by EEPROM.

  • Just read the W25Q128JV datasheet, it uses the DI input pin to write instructions/addresses or data to the device on the rising edge of CLK, and uses DO output pin to read data or status from the device on the falling edge of CLK.

    So you can setup the TMS570 SPI clock polarity and phase to 0 (polarity=0, and phase=0):