This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LC4357: Peripheral interface communication issues(SCI,SPI) when enabled DMA

Part Number: TMS570LC4357

Hi Team,

In Our Application based on the TMS570LC4357 processor, we are having the following DMA channels used for the below-mentioned purpose. Given Table also defines the data rate currently used by the application for establishing the required communication:

Peripheral

DMA Channel

No

Data Rate

Configured Priorities

Functionality in Application

SPI1 Rx

9

Slave Mode with 10MHZ baud rate (32 bit for every 125 ms)

High

Marker Beacon

SCI3 Rx

5

57600 (330-340 bytes for every 100ms)

Low

TE2 tool

SCI3 Tx

4

57600 (301 bytes for every 100ms)

Low

TE2 tool

SCI4 Rx

7

115200 (data size considering the max throughput with the Baud Rate)

Low

GNSS

SCI4 Tx

6

115200 (data size considering the max throughput with the Baud Rate)

Low

GNSS

Here, SPI1 Rx is configured as the highest priority due to its criticality in nature, where we receive the data continuously on this Peripheral.

The Below diagram gives the overview about the Peripheral Interface with the Hercules Processor.

Here, Currently in our application, we are facing issues while receiving the data over SCI3, as mentioned in the earlier tickets provided below the ticket links:

https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/1041094/tms570lc4357-sci-dma-rx-issue-when-same-sci-module-is-enabled-for-tx-over-dma/3905010?tisearch=e2e-sitesearch&keymatch=%25252520user%2525253A484499#3905010

https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/1055928/tms570lc4357-dma-throughput-calculations/3933893?tisearch=e2e-sitesearch&keymatch=%252520user%25253A484499#3933893

As per the reference manual, we tried to configure the round robin scheme for the low priority channels and Fixed scheme for high priority channels. However, the missing of one/2 bytes sporadically for the SCI3 Reception i.e. for the DMA Channel 5 is still there. We had tried changing the priorities of these DMA Channels but it did not help in resolving.

Furthermore as a workaround we have observed that, when the SCI3 tx is switched into the polling mode instead of DMA, that time we are not seeing any kind of  issues for SCI3 reception, which indicates that DMA engine of the processor, is not able to handle this all DMA channels in the system.

We would like to understand why the DMA is not allowing to process all these channels. and wanted to understand what would be the approach to use the DMA in better way such that all these DMA channels will get served properly.

I also have attached the method, which we are using to configure the DMA packets for SCI3.UartDma.xlsx

Request team to help us in providing the correct approach to use all these required peripherals Using DMA.

Regards,
Shivam