Part Number: AM2434
Other Parts Discussed in Thread: SYSCONFIG
Hi,
I am working on the AM2434 and I would like to configure a timer to generate a 110MHz interrupt. This interrupt, would trigger a DMA transfer that would eventually be connected to a DAC via the GPMC.
With the MAIN_PLL2_HSDIV6_CLKOUT clock, that runs at 225MHz, I could do that. In the sysconfig interface, the time allows only a tick period in microseconds. That means that I cannot go faster than 1MHz. Can the timer go faster (around 8 nanoseconds)? Is this a hardware limitation or an interface limitation?
On another subject, I have not found any way to connect the timer interrupt to a DMA trigger? Is there something I miss?
Thank you,
Leo