This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MCRC Occurrence of Reserved Interrupt Condition

Hi,

I am using channel 1 of the MCRC in Semi-CPU Mode at a frequency of 16KHz. I am witnessing an occurrence of a reserved interrupt condition (offset value 0x5) at an approximate frequency of 0.05Hz, that is three of four times every minute.

Please can you give me an indication of what this reserved interrupt condition is. Presumably the set 0x5 to 0x8 are associated with channels 1 to 4, as are 0xd to 0x10 for maybe another reserved interrupt condition.

I would also appreciate advice on what action to take when encountering one of these reserved conditions.

Regards, Tony.