Part Number: TMS570LC4357
Hi Experts,
The Safety Manual list diagnostic IOM3 as always enabled. This would mean, that a write in usermode oder to unimplemented location would result in an ESM 137.
The sligthly confusing part is the existence of the ERR_ENABLE_REG (Error Signaling Enable Register). Judging from the discription, this does not refer to the Error itself, but to an interrupt that gets called when the error occurs. The Problem is, if I wanted to use an interrupt I could use the ESM interrupt that gets called when ESM1.37 is signaled (if enabled).
(Q1) What is the purpose of this register and do I need to turn the error signal to the esm?
Thank you and best regards,
Max