Part Number: AM2434
Hello,
i want to implement the Task Manager for the PRU0_0 but it is not possible.
I set up all Task Manager register and connectet the Task 2 Subtask 0 to the Host Interrupt 12. After the Interrupt occurs, the TS2_STATE filed in the TASKS_MGR_GLOBAL_STATUS register is set to 1h. But looking at the PRU0 Control Register, the TS_ENABLE field is 0. I tried tsen 1 with the silicon version 4 and also the .word 0x32800000 but no changes at all. I have no idea what the problem could be.
Regards
Luca