Part Number: TMS570LC4357
Hi experts,
We are currently looking at the FLA10 DIagmode 5 and FLA11 Diagmode 7 Tests of the Safety Manual. Both test list "Branch to non-flash region" as first step.
Furthermore when executing diagmode 5 there have to be no requests from bus masters.
As far as I can tell this would mean that everytime these tests are executed we need to run them from RAM and disable all interrupts.
This would make running these tests periodicly every few hundred ms realy difficult.
(Q1) Is it necessary to run this test from RAM and disable all interrupts during execution?
(Q2) How often should such a test be run? (1 per System Safety time or every 100h or ...)
Thank you and best regards,
Max