Part Number: LP-AM243
Was an example of the DMA added to the MCU+SDK library? I haven't found it yet but I may have an outdated version. I am looking to add DMA for the on chip ADC so it can have a DMA buffer of ADC read values.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LP-AM243
Was an example of the DMA added to the MCU+SDK library? I haven't found it yet but I may have an outdated version. I am looking to add DMA for the on chip ADC so it can have a DMA buffer of ADC read values.
Hi Dylan,
There is a DMA ADC example in MCU+ SDK for AM243x 08.02.00.28 (it was temporarily removed from TI web site last week, will be restored in this week):
mcu_plus_sdk_am243x_08_02_00_28\examples\drivers\udma\udma_adc_read (Also available in 08.01.00.36)
And there are a few DMA with peripheral examples:
mcu_plus_sdk_am243x_08_02_00_28\examples\drivers\uart\uart_echo_dma and
mcu_plus_sdk_am243x_08_02_00_28\examples\drivers\mcspi\mcspi_loopback_dma
mcu_plus_sdk_am243x_08_02_00_28\examples\drivers\ospi\ospi_flash_dma (Also available in 08.01.00.36)
Best regards,
Ming