This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SPNU495a - STC Control Registers Base Address incorrect



Hello,

in SPNU495a in 14.9 the base address of the STC control registers is given as 0xFFFFF800 however in SPNS157B it is shown as 0xFFFFE400 (CPU STC (LBIST)). So I think the base address in the Technical Reference Manual (SPNU495a) needs to be corrected. Could you please confirm this and take it into account for the next TRM update ?

BR

Andreas

  • You are right. The base address of LBIST/STC in SPNU495a and SPNU489b are wrong.

    For TMS470M, the base address should be 0xFFFFE400,

    For TMS570LS2x, the base address should be 0xFFFFE600  

    In both case, the base address in the datasheet, SPNS157, SPNS141, SPNS159 are correct.

    This mistakes will be fixed in next TRM release.

    Thanks for  finding that.

    Regards,

    Haixiao